configure SPSB081 watchdog
Hello,
We are currently integrating the SPSB081 PMIC for voltage and wake-up management in a Body Control Module (BCM). The PMIC is interfaced with an NXP S32K312 MCU via SPI.
System Setup:
- MCU: NXP S32K312 (100-pin package)
- PMIC: SPSB081
- Communication: SPI
- SPI Configuration: CPOL = 0, CPHA = 0, 32-bit frames
- SPI communication has been verified and basic register read/write operations are working correctly.
Issue: Watchdog Runtime Configuration
We are trying to perform runtime watchdog configuration and set the watchdog window to 160ms. However, we would like to confirm the correct SPI command sequence required for modifying the watchdog configuration during runtime.
Request:
- Confirmation of the correct SPI register write sequence required for runtime watchdog reconfiguration.
- Any recommended configuration example for setting a 160ms watchdog window.
- Debug guidance in case watchdog failures occur when using SPSB081 with S32K312.
Thank you