Skip to main content
AVERM.21
Associate
November 3, 2022
Question

Diode SMB pack body marking "6T C409" is used in protection circuit. Wats to its complete part number

  • November 3, 2022
  • 5 replies
  • 1059 views

Diode SMB pack body marking "6T C409" is used in protection circuit. Wats to its complete part number0693W00000VOorhQAD.jpg

    This topic has been closed for replies.

    5 replies

    Peter BENSCH
    Technical Moderator
    November 3, 2022

    Welcome, @AVERM.2​, to the community!

    ET = SM6T33A

    Good luck!

    Regards

    /Peter

    AVERM.21
    AVERM.21Author
    Associate
    November 3, 2022

    Thanks Peter Bensch for your prompt response and confirmation of ST part no.

    Peter BENSCH
    Technical Moderator
    November 3, 2022

    You're welcome!

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter

    AVERM.21
    AVERM.21Author
    Associate
    November 4, 2022

    Based on above response, I ordered this part Diode # SM6T33A. I trust that part no shared is 100% correct. Once received, will mount on PCBA and bring up. Once all ok, will share my response and consider this as closed.

    Peter BENSCH
    Technical Moderator
    November 4, 2022

    If you are repairing a PCB where the TVS has been destroyed by an overvoltage pulse, you should also check the components around it. The TVS is supposed to survive such impulses, but the impulse energy was apparently greater, so that other components or the entire unit may have been affected.

    Good luck!

    /Peter