Skip to main content
Visitor II
October 10, 2024
Question

Discrepancy in CFG_2.FR_ADJ bit values between Table 12 and Table 18 in L9800 Datasheet

  • October 10, 2024
  • 1 reply
  • 825 views

Hello,

I have a question regarding the L9800 product (LS driver). The value of the CFG_2.FR_ADJ bit in "Table 12. Coefficient overview" differs from the value of the CFG_2.FR_ADJ bit in "Table 18. Register addressing space" in the datasheet. Could you please clarify which value is correct?

 

* Table 12. Coefficient overview

swbae_1-1728547763537.png

* Table 18. Register addressing space

swbae_0-1728547737057.png

Thank you.

1 reply

ST Employee
October 18, 2024

Hello,

 

you are right, there is a mismatch between table 12 and table 18. The right values are the ones inside the table 12.

Our team will change the datasheet information included in the table 18.

thanks

Giulia