Question
Do I need to use a Freq to Voltage converter for a tacho signal from 4 wire fan?
Hi all,
I am using a 4-wire fan supplied by 24V. I was wondering if the tacho output from the fan needs an external timer or a Freq to voltage converter; or can I just use a pull up resistor and connect the tacho signal straight to the input of STM32 using one of its internal Timer.
I appreciate your help!
Regards,
Sabrine