Associate
October 7, 2020
Solved
EVALKIT-ROBOT-1 / MODBUS RTU / QUESTION
- October 7, 2020
- 3 replies
- 1848 views
Hello Community
I try to test the EVELKIT-ROBOT-1 using MODBUS RTU.
I did it it's factory setting.
After I had connect all the cables, I powered up the EVALKIT.
Motor turned to its init position and stoped at some point.
And Motor hold that position even if I turned the sharft of the motor.
So I want to change the desired posiiton.
I send packets(? : I don't know whether MODBUS RTU also called it packet ) to the EVALKIT as you can see the figure that I uploaded.
The order that I send was (1) -> (2) -> (3) -> (4) -> (5) -> (2) -> (1) -> (6) -> (7).
Following response is the bottom side of figure.
here is my questions.
- I send packet(1) to EVALKIT after the motor aligned but the response implys it is not. why?
- is packet(7) wrong? ( Set the coil bit 0 at address 0 high to start motion ) Is it because of the discrete input bit 0 is not high?
please help..
Thanks
Minsoo