Fail Safe Mode for Trisils
We are considering using ST TRISIL (TSS) devices for crowbar protection . We have been using an alternative type of protection device from LITTELFUSE (SIDACTOR) in an application where we require the TSS to fail as a short circuit. In our application we require the TSS to be a single use device that fails to a very low impedance in a current limited circuit (~3A) . The LITTELFUSE devices have been tested extensively in our circuit and do fail safe to a very low impedance of ~0.1 ohms however some other brands (not ST) have a percentage that fail with impedance of say 5-7 ohms which is too high a resistance with 3A flowing and this creates excessive power and fire risk. The ST data for the SMP100LC series of TSS device says that it will fail safe and our testing on 10pcs so far shows this to be correct. Can anyone confirm that the design of the TRISIL device will never fail in a higher impedance manner therefore minimizing fire risk?