FOC Motor SDK: Understanding STARTING_ANGLE_DEG in Sensorless Startup Mode
Hello,
just a short question: In Sensorless Mode the startup sequence works with "Align Step", where the Rotor starts from a fixed position. There is a define for the Motor Startup Angle (STARTING_ANGLE_DEG)... Is it relevant if there is 90 ° or 0 ° entered?
We decide it to have 0 °, because there is a math operation with the rotation direction. (multiply -1 or 1 to the angle) and with 0, we get always the same start condition.
Whats the purpose of this Parameter in Sensorless Mode? Could it we do it wrong and have a performance decrease?
Best regards
Sebastian