How to tune FOD parameters on the STWBC IC.
I'm using the STWBC as the IC to control the transmitter of a wireless battery charger. So far the battery is charging fine but I am unable to get foreign object detection working. I am adjusting the FOD parameters using the STWBC GUI application. Is there a documented procedure on how to optimize the FOD values?
Either FOD errors occur randomly when there is no foreign object or no FOD error is given when a foreign object is there, depending on the parameter values. The STWBC GUI does show the RX report power drops significantly when I place foreign objects in the way. This leads me to believe it is only the FOD parameters that are the problem.