Skip to main content
JAKE2
Associate III
July 11, 2023
Solved

I am Finding wireless charging guru ▶ Heat comes out while Wireless charging.

  • July 11, 2023
  • 8 replies
  • 4020 views

Hello everyone !

I am using STWBC86 and STWLC38 MCUs, using our own custom board.

The wireless charging was going well, but the problem is this.

[ When charging → put away the RX → put back the RX ] ...▶ the heat comes out from the RX MCU.

Any ideas to solve this issue ? Thank you.

This topic has been closed for replies.
Best answer by Didier HERROUIN

Hello,

The output voltage from STWLC38 is not supposed to oscillate, it should be stable as it is a LDO output.
Could you attach a zoom of the period of time where VIN2=5V and then it falls ? It is difficult to see on the plot the behavior of VIN2 and if it exceeds 5.5V.
If you suspect a overvoltage protection by TPS2116, you could try (for testing purpose) to set Vout=4.5V using STWLC38 GUI.

Then, which configuration do you use inside STWLC38 ? I understood that you have modified several parameters, it may be a reason of instability. For instance, if you have increased the minimum operating frequency, you will get less power available at Vout. In your 3rd case, have you tested that Vout is still stable when you draw some current ? 
What is the maximum of power that you need at Vout ?

Regards,

Didier

8 replies

JAKE2
JAKE2Author
Associate III
July 13, 2023

While catching up the Qi. V.1.3 contents, the Tx will not transfer power untill the "Ping ▶ Configuration ▶ Negotiation" protocol cycle, then where would the Tx's transmit power go during these process?

I am assuming that these power (during protocol phases right before Power Transfer) are going to dissipate into heat, from the internal part of RX IC. 

JAKE2
JAKE2Author
Associate III
July 13, 2023

When using STWBC86 and STWLC combination, the charging is excellent.

No heat comes out from TX's side, neither as well from the RX's side, when charging as usual.

The heat problem occurs when I intentionally repeat attaching and dettaching so many times

(to be precise, I am making problem intentionally , to secure the safety of heat comes out for some reason

And while I'm reading Qi. V.1.3 document, I got insights, those are..

To maximize TX PING DURATION, and to minimize TX PING INTERVAL.

It worked pretty well, but still heat comes out from RX. 

I am not sure my experiment is going well, are there somebody in similar case ?

JAKE2
JAKE2Author
Associate III
July 13, 2023

To reduce heat, I changed two parameters on the TX's side, using GUI.

① I changed the TX frequency from around 146kHz to 160kHz (the heat reduced, much better. But it needs additional modification to handle the heat issue, because the heat still comes out)

Using frequency above around 170kHz, cannot charge to my custom board.

I think the frequency and  power efficiency are trade-off-relationship.

② I changed the re-ping delay parameter from 1,000ms to 300ms

The register is located at Tx Registers ▶ Tx Configuration ▶ "TX PING INTERVAL" register.

The interval of heating issue has reduced, but there is still heat, at times. And I do not know what side effect will happen. 

JAKE2
JAKE2Author
Associate III
August 2, 2023

While I am looking around RX Configuration Qi, what is RP24 ?

I had been heard about RP or RP8, but never heard of RP24. Could you tell me what is it ?

+) It seems like my wireless charging set is not ready for EPP, because it can not reach to negotiation phase

(TX PTC UPDATE LTCH is always "Did not occur" - status)

I wonder the Qi 1.2.4 Tx and Qi 1.3 Rx is compatible to coply EPP ▶Negotiation and Renegotiation

Sincerely Yours,

Jake Kang

JAKE2
JAKE2Author
Associate III
August 4, 2023

I just happend to found out the reason for Rx heating, it was because I set too high voltage for ARC threshold.

I changed the setting from 6V(original value) to 4V(new value), and the problem was wiped out, it works well.

JAKE2
JAKE2Author
Associate III
December 27, 2023

Now I am facing the problem regards to using power Multiplexer, get input two inputs separately( Wireless charging voltage , USB-C Type 5VDC) and outputs the single supply among the two inputs.
The problem is, as far as I understand, the wireless charging's output voltage does fluctuates so hard while Mux's safety input voltage range is narrower than the former, so the Multiplexer seems constantly continues resetting on and on.

I will attatch very simple diagram of the Multiplexer IC ( It's made from another company, but I guess you well aware)

wireless_wired--powerMux.jpeg

I've tried connecting directly the wireless charging's output node into the Load, removing the power mux IC, and it worked.
Does anyone developed wireless charging with the option of using USB type wired charging as well?

Or could you recommend the power Mux that can possibly use with wireless charging IC ?

Sincerely Yours, Jake Kang.

JAKE2
JAKE2Author
Associate III
January 2, 2024

20240102_TSP2116_TEST_JAKE.png

I have tested three different case, could anyone recommend a power mux IC instead of TPS2116 ?

Didier HERROUIN
Didier HERROUINBest answer
Technical Moderator
January 2, 2024

Hello,

The output voltage from STWLC38 is not supposed to oscillate, it should be stable as it is a LDO output.
Could you attach a zoom of the period of time where VIN2=5V and then it falls ? It is difficult to see on the plot the behavior of VIN2 and if it exceeds 5.5V.
If you suspect a overvoltage protection by TPS2116, you could try (for testing purpose) to set Vout=4.5V using STWLC38 GUI.

Then, which configuration do you use inside STWLC38 ? I understood that you have modified several parameters, it may be a reason of instability. For instance, if you have increased the minimum operating frequency, you will get less power available at Vout. In your 3rd case, have you tested that Vout is still stable when you draw some current ? 
What is the maximum of power that you need at Vout ?

Regards,

Didier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JAKE2
JAKE2Author
Associate III
January 24, 2024

I started increase the load, from 100mA to 1,000mA in 100mA step. The Vout remains stable.

For our product, power could be 1.35 ~ 2.5W or so (300~500mA , by setting Vout 4.5 V - to 5.0 V).

I have to test further, but it seems the problem solved.

Thank You.

 

JAKE2
JAKE2Author
Associate III
January 3, 2024

Case #1, USB OFFCase #1, USB OFFimage.pngimage.pngimage.png

JAKE2_2-1704264458690.png

JAKE2_3-1704264463574.png

↑ Here's the zoomed Waveform.

Then, which configuration do you use inside STWLC38 ?

RX ARC THRES = 6.0V → 4.0V

RX BPP VOUT SET = 5.0V → 4.5V

when adopted  the voltage that you metioned, the it works well to do so.

 

In your 3rd case, have you tested that Vout is still stable when you draw some current ? 

→ I haven't tested yet, it just starts working fine from today. 

 

Thank You