Skip to main content
ALumb.1
Visitor II
March 27, 2023
Question

I am looking for a replacement of the Renesas driver HIP4086ABZ, 3-phase N-channel MOSFET drivers, specifically targeted for PWM motor control with a package size equal or lower. Thanks for your proposals

  • March 27, 2023
  • 1 reply
  • 789 views

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    Technical Moderator
    March 27, 2023

    Welcome, @ALumb.1​, to the community!

    You could either look at the STDRIVE101 with max 75V bus voltage, alternatively the STDRIVE601 for 600V.

    You can get more help from your local FAE or ST office.

    If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

    Regards

    /Peter