I'm using the STC4054 Li-ion single cell charger in a design, the CHRG pin is supposed to have a weak pull-down when not charging but the current drawn is higher than specs
In the STC4054 datasheet, it says the CHRG pin is supposed to have a weak pull-down of max 35uA when no battery is connected yet. However, with a 4.7Kohm pullup from that pin to 3.3v, I measure a 1.2v drop, which indicates about 250uA of current. With a 390 ohm pullup, the drop is about the same, which indicates almost 10x the current. Am I misunderstanding something on the datasheet? Thanks!