I want to know if there are different housings used for BTW69-1200? I have 2 devices on my table and wonder if ST has used also a different housing and if there are any differences between the devices?
I want to know if there are different housings used for BTW69-1200? I have 2 devices on my table and wonder if ST has used also a different housing and if there are any differences between the devices?
Yes, I mean the notches on the leadframe on the back. They do not have the same marking on the front side. One must be 10 years older (the one without G)
The additional marking G for Halogen Free = Green was introduced in 2008, the Product Information Letter "PIL CRP/08/4251" can be found using your preferred search engine.
Would the notch have a significant impact on the mechanical mounting or cooling in your project?
Hello Peter, thx for your answer. Seems the device is from the year 2000 then, because it has no G and date-code is 032. The question for me is if I can take them and they are as good as new ones? I hope nothing important (with cooling etc) has changed in the last 20 Years? Best regards Lothar