ISO808 Fault status
During a short circuit of the ISO808 channel output (+28V) to ground, the fault status shows a voltage between 0.8V and 1.4V instead of 0V. When the short is removed, the fault status reads 3.3V. A 1k pull-up resistor is connected to the fault open-drain pin. Due to this voltage level, the microcontroller is unable to correctly detect the low state for fault status. how to get 0v on fault pin during the short circuit time.