Skip to main content
Visitor II
May 8, 2024
Question

L4986 startup problems with external VCC supply

  • May 8, 2024
  • 0 replies
  • 469 views

I am evaluating a PFC with the EVL4986-350W evaluation board.

To be able to use Boost coils without the extra winding I want to supply the VCC voltage from a buck converter connected to the output voltage. The voltage from the buck is 17V.

I have tried to connect the buck directly to VCC capacitor and wia the diode (D7) to VCC. C9 was disconnected.

Why doesn't the PFC  start up?

It start up if I connect the VCC voltage after the AC power but not if the VCC is powered up before or at the same time as the AC-input.

This topic has been closed for replies.