L6472 output voltage detected on motor supply
Hello,
I have a board based on the stepper driver L6472. I noticed that, when I do not provide input 12V for the motor (the motor 12V but I provide the 3.3V for the logic (VREG, VDD, SW), I find a voltage of about 2.6V on the VSA, VSB pins.
I tried to exclude all other possible source on the board and I think that this voltage is produced by the L6472. To have a definitive confirm I should cut some PBC track. Before doing this I would ask if it is an expected behaviour (to have 2.6V at motor output).