L7987 ripple issue
HI Sir,
we have two different results of the ripple noise
base on same PCBA design, but different L7987 origin:
1. Mark of "ST e3 G9207,L7987, CHN 3L0",ripple noise 2.2V 2.9KHz
input 24V, output 12V, load 5ohm 2.4A
2. Mark of "ST e3 7B658, L7987, PHL 037",ripple noise 0.04V
input 24V, output 12V, load 5ohm 2.4A
the image of the chip and the image of the ripple see below.
why is it like that, it make no sense,
could you please advise.
thanks.
with best regards,
PZha
L7987 CHN 12V 2.5A, 24V in
L7987 PHL 12V 2.5A, 24V in
L7987 CHN
L7987 PHL