Skip to main content
Associate II
January 15, 2026
Question

L9026 incorrect response on MISO

  • January 15, 2026
  • 3 replies
  • 444 views

Original title: MOSI is not responding in SPI interface TI C2000 MCU & L9026

Edited for clarity.


Hi All, 
We are having SPI interface between TI C2000 MCU (TMS320F28P659DK8-Q1) and High Side Driver(L9026) the Our Target Board. Here are some observations regarding SPI communication. MISO(L9026) is not responding, not giving 
  1. We are able to send data in L9026 & MISO is responding.
  2. Supply voltage of VDDIO=3.3V, VBATT=12V, IDLE (HIGH)=3.3V, IN0(HIGH)=IN1(HIGH)=3.3V,(All voltages are within the limit as per L9026 datasheet). I have attached the logs for that.
  3. We Sent in MOSI CFG_1: 0x8900 (put device in active mode, frame counter = 0).
  4. We sent in MOSI STA_1:0x4403 , but the response is 0x2201, not able to read device status register.
  5. We also checked in Idle mode too Supply voltage of VDDIO=3.3V, VBATT=12V, IDLE (HIGH)=3.3V, IN0(LOW)=IN1(LOW)=0V, in all the cases response not able to read device status register. I have attached the logs for that.
  6.  We also checked with IN0 = 0, IN1 = 0, IDLE = 0. then  The device is in sleep mode, then IN0 = 0, IN1 = 0, IDLE = 1. The device is in idle mode
    SPI initial configuration:(similar to EVK board)
    – CFG_0: 0X8420 (configure CH3 as HS, all other outputs are in default state LS, frame
    counter = 0))
    – MAP_IN0: 0x9C05 (associate IN0 to CH0, frame counter = 1)
    – MAP_IN1: 0xA080 (associate IN1 to CH5, frame counter = 0)
    – CFG_1: 0x8803 (LED PWM generator freq = 122.5Hz, frame counter = 1)
    – CFG_2: 0x8C00 (GEN PWM generator freq = 122.5Hz, no adjustment, frame counter = 0)
    – PWM_LED_DC: 0xB001 (PWM LED duty cycle = 0%, frame counter = 1)
    – PWM_GEN_DC: 0xAC02 (PWM GEN duty cycle = 0%, frame counter = 0)
    – MAP_PWM: 0xA431 (CH2-CH3 driven by internal PWM generators, frame counter = 1)
    – PWM_SEL: 0xA812 (CH2 driven by PWM LED & CH3 driven by PWM GEN, frame counter = 0)
    – BIM: 0x9041 (activate bulb inrush mode on CH4, frame counter = 1)
    – CFG_1: 0x8900 (put device in active mode, frame counter = 0)
    – STA_1:0x4403 (we got response as 0x2201)
    – DIAG_OFF_EN: 0xB7FF 
    – STA_0: 0x4000 
    – DIAG_OPL_OFF: 0x4C01 
    – DIAG_SHG: 0x5400
     IN0 =1, IN1 = 1(done here)
    – PWM_SPI: 0x9B49 (all SPI driven channels are switched ON, frame counter = 1)
    – PWM_GEN_DC: 0xAFFE (configure PWM GEN duty cycle at 100 %, the expected effect is CH3
    fully ON, frame counter = 0)
    – PWM_LED_DC: 0XB3FD (configure PWM LED duty cycle at 100 %, the expected effect is CH2
    fully ON, frame counter = 1)
    – DIAG_OVC_OVT:0x4802  
    – DIAG_OVC_OVT_RLW: 0XBFFD
    DIAG_OPL_ON_EN: 0xB804 
    – DIAG_OPL_ON_EN: 0xB809 
    – DIAG_OPL_ON_EN: 0xB820
    – DIAG_OPL_ON:0x5003 
    In this case also we got the response 0x2201. 
    I have attached all logs in L9026 .7z zip file.
    Quick response will be greatly appreciated.

3 replies

Andrew Neil
Super User
January 15, 2026

@Dharam wrote:
 MISO (L9026) is not responding

Your thread title says, "MOSI is not responding" - is that a typo ?

But your logic analyser traces show activity on both MISO and MOSI !

 

Please show the schematic of how you have the L9026 connected to the MCU.

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
DharamAuthor
Associate II
January 15, 2026

Dharam_0-1768475399230.png

when we are giving (IN0=IN1=0V & IDLE =3.3V ) OR (IN0=IN1=3.3V & IDLE =3.3V), in both cases We are sending data in MOSI ( checking STA1  register- Global Base Address + 0x11) 0x4403 , Slave device (MISO) is responding as 0x2201.
Quick response will be greatly appreciated.

DharamAuthor
Associate II
January 15, 2026

We are getting data in MISO as you mentioned. but It should be correct. We are not able read proper Device id & Status register (Data sent by Slave device (MISO) ).  


Title edited to reflect this.

TDK
Super User
January 15, 2026

Your master has incorrect CPHA=1. Data is changing on rising edge, it should be changing on falling edge.

TDK_0-1768483703260.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
DharamAuthor
Associate II
January 16, 2026

Hi, Thanks for your response. Now L9026 is working. one observation, when we are sending MOSI 0x4403, in MISO response is showing 0xC4CC(1100 0100 1100 1100) . 1 ERR error bit, ‘1’ if an error happened in the previous transmission. What type of error is happening ?
I have attached log & zip file for your reference. 

Dharam_1-1768543492236.png

 

Andrew Neil
Super User
January 16, 2026

@Dharam wrote:

Now L9026 is working.


Excellent. So please mark the solution - on the post which provided the answer (not this one).

 


@Dharam wrote:

when we are sending MOSI 0x4403, in MISO response is showing 0xC4CC(1100 0100 1100 1100) . 1 ERR error bit, ‘1’ if an error happened in the previous transmission. What type of error is happening ?


That's a new question - please start a new thread for that.

Post a link here to your new thread

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.