Question
[L9369] Reg 6Fh D[1] =0 to set Low ohmic path to be connected or disconnected?
Register 6Fh, D[1] SPI_HSoff_high
Low ohmic path switch off disable bit for HS pre-driver stage A and B
0 / R/W (default) (‘1’ = low ohmic path enabled)
When D[1] =0, Low ohmic path between HS driver GHy_x and SHy_x is connected or disconnected?
When H-bridge output to driver motor running, should Low ohmic path be connected?
Thanks!