Associate II
September 16, 2023
Question
LED2001 no output
- September 16, 2023
- 1 reply
- 1521 views
Dear Support and Expert,
We are using LED2001 to drive a LED, 2V@4A. the 6 boards come back. 4 work good but 2 no output voltage. we are using QFPN package, is there a way to check the pins are properly soldered beside take it out and reinstall? 2. is it possible that the components and layout make the driver working in a marginal area? in our case, the design seems working but not good. how to optimize the design from the schematic point of view? I will pay attention when we do the next layout.
Thank you,
David