Need Clarification On The Relationship Between INPUT and OUTPUT Pins for VNQ9025AJ
I know this is a really dumb question, but I cannot find a definitive answer in the datasheet for the VNQ9025AJ, Quad channel high-side driver with Current Sense analog feedback for automotive applications.
There are 4 pins called INPUT0 to INPUT3. There are 4 output pins called OUTPUT0 to OUTPUT3. I just want to verify that when INPUT0 goes to a logic 1 value, that OUTPUT0 is activated (i.e. current is flowing).
I would also like to know if the input/output relationships are independent of each other. In other words, can I have INPUT0 and INPUT1 high at the same time with current flowing in OUPUT0 and OUTPUT1 at the same time? Or, can there only be one active input/output pair at a time?
The datasheet says
"Voltage controlled input pin with hysteresis, compatible with 3 V and 5 V CMOS outputs; controls output switch state."
"controls output switch state" is a bit vague, IMO. it is also confusing to see the 4 CS output states controlled by 2 multiplexed control lines, whereas the 4 output lines seem to be controlled by 4 input lines.