Visitor II
August 2, 2023
Question
Negative Triac supply
- August 2, 2023
- 1 reply
- 1804 views
Hi,
I have a requirement to drive a Triac from the MCU powered by a DC/DC converter. The AC supply is typ 24 VAC @ Rc terminal with respect to C terminal. The Triac is to be driven as attached. The MCU GND should always regulated at Rc - 3V3. The MCU output which drives the gate preferably will be connected straight, without the BJT. The gate current is II/III quadrants is typ 5 mA.
How do I configure a buck regulator and its input to achieve this?
Cheers,
Kaushalya