Output capacitor type for use with LD1117
Dear Forum members,
Could you please confirm if the LD1117 is specified to work with ceramic output capacitors?
Unfortunately the datasheet makes no mention of capacitor type or ESR requirements.
Thank you
Dear Forum members,
Could you please confirm if the LD1117 is specified to work with ceramic output capacitors?
Unfortunately the datasheet makes no mention of capacitor type or ESR requirements.
Thank you
Welcome, @Bvan .11, to the community!
The LD1117, which is quite 20 years old, is a low-dropout regulator that requires an output capacitor of at least 10µF and an ESR (equivalent series resistance) of at least 0.3 ohms. 20 years ago, they simply used an electrolytic capacitor whose ESR was large enough. In addition, the large capacitance values of ceramic capacitors were not yet available at that time, so they were not mentioned in the data sheet.
If a tantalum capacitor is out of the question (there is massive criticism of the circumstances of tantalum mining), you can also use a ceramic MLCC, but then you should connect a resistor of approx. 0.5-2 ohms in series as an artificial ESR.
Does it answer your question?
Regards
/Peter
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.