Skip to main content
ny851
Associate II
August 31, 2023
Question

output current of ISO808

  • August 31, 2023
  • 1 reply
  • 1090 views

hello 

we are going to use ISO808 IC in our project according to the datasheet of ISO808 Short circuit protection on output channels ( ILIM(MIN) )is 0.7A but for Channel Output Current (continuous) it is mentioned as internally limited. could you please provide a data for continuous maximum output current per channel at 25 C ambient temperature or Is there any formula to calculate per channel continuous output current at particular ambient temperature. 

Best regards,
Nisha Yadav

This topic has been closed for replies.

1 reply

ny851
ny851Author
Associate II
September 6, 2023

Hello Team,

Any update on this?