Skip to main content
Associate
October 4, 2023
Question

Overvoltage suppresion by clamping circuit in IGBT driver

  • October 4, 2023
  • 1 reply
  • 1053 views

I am designing clamping circuit for IGBT driver. The max voltage is 4800V. I was thinking about using STTH112A diode. In the datasheet, there is no information about thermal resistance - junction to ambient for SMB or SMBflat version. How can I assess the number of diodes I need to use and what is the maximal Vrrm of the diode which can be used in these circuit? Is STTH112A suitable for these design?

 

This topic has been closed for replies.

1 reply

DCISS.1
ST Employee
October 10, 2023

Hi "Perpot", 

The Thermal resistance junction to ambient for SMB is available in datasheet  figure 6. For minimum footprint the Rthja = ~ 105°C/W (from figure 6). To withstand your maximum voltage 4800V, I advice you to use 5 diodes in series 6kV in total (with a derating of 80%). For each diode, you will need to put in parallel a resistor and a capacitance. Both are in parallel with the diode. R <= 1MOhm and C>= 200pF (C is defined for a didt = 100A/us, Qrr = 289nC, Irm = 3.8A at Tj = 125°C).

To reiterate the calculation, you case use this application note AN443.

Best regards, 

D.CISSE

perprotAuthor
Associate
October 11, 2023

Hi DCISS.1,

Thank you so much for your replay. I've missed this information.

If we will take Rthja = ~ 105°C/W, working temperature = 65°C and max operating temp = 175°C then max allowed power per diode is (175-65)/105 = 1.05W.

Vbr=4800V, inrush current 3.9A, inrush time 10us, inrush interval 10000us, we can calculate average Pd = 4800*3.9*10/10000 = 9.6W

so, we need 9.6/1.05 = 9.2 diodes with Vbr = 4800/9.2 = 524V

According to your advise we need 5 diodes with Vbr 1200V.

I am not sure which calculation can be used for the clamping circuit design. Any advise, please?

Kind regards,

perprot