Question
PowerStep01 application: Specify number of steps for RUN command ?
Hi,
I have a question about the RUN command because there are different speed to MOVE command.
In RUN command the speed min its 0,015 Step/second , in MOVE command the max speed min it is 15.25 Step/Second.
I need run the motor at very low speed similar to RUN command but i need set the number of step.
Are there a solutions ?
Thank you.
Giorgio Tessari