PWM current LED PCB with STCS2A
Dear all,
I received a LED PCB with 16 STCS2A constant current LED drivers in parallel, each powering 4 LEDs. Vcc=12V, for the PWM signal a 5V signal is used, which is supplied as follows: 24V PWM output of PLC is coupled to an optocoupler which is connected to a 5V power supply, the 5V output of this optocoupler is fed to the PWM input of the STCS2A drivers. When testing the system the 5V PWM signal shows high current values up to 1A, luckily this was protected with a glass fuse. What could be causing this problem?
Happy to hear any idea's or useful things to test, the PCB is not my own production and I am trying to explain/solve the issue.
Best,