Skip to main content
Associate
March 12, 2024
Question

Question for Application note AN5734.

  • March 12, 2024
  • 2 replies
  • 1100 views

My company designs circuits and artwork upon request from customers.

We are considering this project based on a customer's request to change the laser power supply to be compatible with worldwide use.

While considering various things, I am also considering a PFC circuit with L4985.

Question for Application note AN5734.

AN5734 : Table 4 on page 27

Is the relationship between Wire type and Wire diameter correct?

----------------------------------------------------------------------------------------------------------------------

Windings   Start pins   End pins    Number of turns        Wire type           Wire diameter

 PRIM              5               2                     70                  Single – G2         Litz 0.2Ø x 30

 AUX                9             11               5 (spaced)            Litz – G2                0.28Ø

----------------------------------------------------------------------------------------------------------------------

Do you have any information on transformers?

Best regards.

This topic has been closed for replies.

2 replies

Peter BENSCH
Technical Moderator
March 12, 2024

Welcome @shinba, to the community!

Why exactly do you think the information on wire diameter and wire type is incorrect?

Regards
/Peter

shinbaAuthor
Associate
March 13, 2024

The wire type on the PRIM side is single Grade 2, but the wire diameter is Litz wire.

Also, the wire type on the AUX side is grade 2 Litz wire, but the wire diameter is 0.28Φ.

Is this correct.

Best regards.