Associate II
November 10, 2023
Solved
Solar charging and autonomous power supply for MCU
- November 10, 2023
- 2 replies
- 2886 views
Hi All,
I'd like to create a PCB for my school project that captures energy from a small solar panel using SP1040. The harvested energy will then be used to charge a LiFePO4 battery (3.6~3.7V) through the LD6924 battery charger. Additionally, the voltage will be regulated to supply power to the MCU VDD. My ultimate goal is to construct a completely autonomous outdoor wireless module powered by solar energy. I've consulted various reference designs and product datasheets to develop the following schematics. I would greatly appreciate it if you could review it and provide feedback on potential improvements or identify any mistakes in the implementation.
Best regards,
Levan