ST1S12G18R Output Voltage Issue - Feedback Not Functioning Properly
- July 29, 2025
- 2 replies
- 379 views
Hello,
I'm encountering an issue with the ST1S12G18R DC/DC regulator. I've attached the reference schematic from the datasheet and my PCB layout, created in Altium. As you can see, my design matches exactly with the reference schematic provided by ST.
According to the datasheet, with approximately 5V input and the recommended reference schematic resistor values, I should obtain 1.2V at the output (56k ohm resistor used for both feedback resistors). However, I'm consistently measuring around 4V instead of the expected 1.2V.
Because I specifically need a 3.3V output in my design, I adjusted the feedback resistors to 150 k ohm and 33.2 ohm. Still, the output voltage remains stable at approximately 4.3V when the input voltage is in the range of 4.5V to 6V. Only when the input voltage drops below 4V does the output voltage start decreasing accordingly. This behaviour indicates to me that the feedback loop may not be actively controlling the output voltage as intended.
To further investigate, I reduced the feedback resistor from 150k to 100k, yet the output remained unchanged at 4.3V. Changing the feedback resistor values does not seem to affect the output voltage.
Additionally, I performed another test by leaving the output open-circuited (no load). Under these conditions, the output directly reflects the input voltage, further suggesting the feedback control loop is inactive.
I have five identical PCBs, and all show this same behaviour. Thus, it's unlikely to be related to a faulty component or assembly error specific to one board.
Could you please advise me on how I can properly achieve a stable 3.3V output from this regulator? Any recommendations or insights into resolving this feedback issue would be greatly appreciated.
Thanks in advance for your assistance.