Skip to main content
Associate
January 14, 2024
Solved

STBC15 output current?

  • January 14, 2024
  • 4 replies
  • 1175 views

Hi all,

I recently stumbled upon STBC15 and I am interested in integrating it into our next design. However, I am lacking a critical parameter from the datasheet: what is the typical and maximum allowed current flowing from VBAT to the OUT pin?

This topic has been closed for replies.
Best answer by Peter BENSCH

Sorry, I hadn't read your question correctly. The maximum current for the M3 transistor is indeed not specified, but it results from the intended applications.

The LiIO batteries typically used in low current applications are not only charged with max 1C, but normally also discharged with max 1C.

In the data sheet, table 5, you will find the Rdson of the transistors M1...M3 = 3 ohms,  i.e. all identical parameters. Because this Rdson generally determines the maximum current in the FET, this results in the same maximum current of 40mA as the max charging current.

When selecting the current through M3, please bear in mind that its power dissipation increases quadratically with the current.

Regards
/Peter

4 replies

Peter BENSCH
Technical Moderator
January 14, 2024

Welcome @icharala, to the community!

depending on the configuration of the pins ISET0 and ISET1 this charge current is either 10mA, 20mA, 30mA or 40mA (see data sheet, table 8).

Hope this answers your question?

Regards
/Peter

icharalaAuthor
Associate
January 14, 2024

Hello @Peter BENSCH and thank you for your quick response! This is the charge current (from charge input towards the battery) and this is clear.

 

But from what I see the component has a power path from the battery towards OUT (when the transistor M3 in on and there is no voltage on CHGIN). I am asking for the recommended/maximum current on that path.

 

I guess a safe assumption would be "no more than the charge current" but I am curious if there is any chance to be bigger than 40mA...

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
January 15, 2024

Sorry, I hadn't read your question correctly. The maximum current for the M3 transistor is indeed not specified, but it results from the intended applications.

The LiIO batteries typically used in low current applications are not only charged with max 1C, but normally also discharged with max 1C.

In the data sheet, table 5, you will find the Rdson of the transistors M1...M3 = 3 ohms,  i.e. all identical parameters. Because this Rdson generally determines the maximum current in the FET, this results in the same maximum current of 40mA as the max charging current.

When selecting the current through M3, please bear in mind that its power dissipation increases quadratically with the current.

Regards
/Peter

icharalaAuthor
Associate
January 15, 2024

Gotcha, that makes sense.

And yes, I can estimate the power dissipation from the resistance. Would be nice to know the absolute maximum though :)