STEVAL-BMS114TX no signs of life
Hello,
I am looking for an IC to monitor cell voltages of a 12s lipo battery.
I found the L99BM114 IC. To get started, I bought the STEVAL-BMS114TX.

Currently, I have connected 12 resistors in series to my lab supply with 48v. In between these resistors, I soldered cables and connected them to the Connector 7 (P1). On Connector 5 (CN1) I connected an STM32 Development MCU. With that MCU, I try to communicate via SPI. On Connector 2 (CN3) I connected my MCU: GND to GND, VIO to 3V3 and VDD to 5V.
My Problem is that I don't get any sings of life from that board via SPI. The Cellcoltages measured at the PCB are correct. I also tried to pull pin20 (SPIEN) of the IC to VCOM, but this doesn't help. Can you give me a point where I can start?
Kind regards and thanks in advance
Dennis