STP24DP05 IC queries
Hi Team,
We are using this STP24DP05 (24-bit constant current LED sink driver with output error detection) IC for a X*Y array of diodes to get high or low. The IC is interfaced with microcontroller using SDI pin of STP24DP05. We have some doubts kindly check-
1. How will the serial pin data transfers to outputs R/G/B pin? does R1 , G1 & B1 gets data first then it goes to next R2,G2,B2? or it will first give data to R1-R8 then to next 8 bits goes to G1-G8 like that.
2. Is LE/DM pin working as reset to all the pins? does the outputs of STP24DP05 gets refreshed when LE/DM is pulled down?
3. Can we keep OE pins as grounded ?