STPMIC1 BSTOUT Continous output current
Hello,
In the STPMIC datasheet, the BSTOUT continous current is specified as being greater than 1.1 A when 3.3 V < VIn < 5.5 V.
If the voltage Vin is greater than 4.5 V, does the BSTOUT continous current increase?
I assume so, since the inductor's peak current limit (IBSTLIM) is 3.3 A and the short-circuit current (IBSTSH) is 4 A, but could you confirm this for me?
If so, what is the BSTOUT continous current when Vin>4.5 V?
Best Regards.
Sylvain