STSW-GMBL02V1 cannot connect
Hi Team.
I'm trying to connect STEVAL-GMBL02V1 board with STSW-GMBL02V1 control application.
The cursor icon becomes a standby animation, but I cannot connect.
I connected using the following steps:
- supply 8V of power to the STEVAL-GMBL02V1 board.
- connect the USB.
- start up the STSW-GMBL02V1 application.
Condition:
- Motor is not connected yet.

The thing to be concerned about is that when you connect USB, the current value decreases.
I am using a power supply that can only display up to two decimal places, but 40mA is displayed as 0A.
I would like to know if the board is defective or if there is a problem with the procedure.
Has anyone experienced a similar problem?