Question
STUSB4500 Default PDOs without I2C
Hi,
We like to use the STUSB4500 without having it to progamm via the I2C. So we need to use the standard configuration. If I understand well, these are has 3 PDOs: 5v/1.5A - 15V/1.5A and 20V/1A.
However, the 20V/1A is too high. Is there a way to prevent the 20V/1A. and to only have the two PDOs 5v/1.5A - 15V/1.5A active. (without to programm the I2C)
Thanks,
Olaf