Skip to main content
Visitor II
May 22, 2024
Solved

STWBC86 GPIO for LEDs

  • May 22, 2024
  • 1 reply
  • 886 views

Hi,

When STWBC86 is operating fully independently without being interfaced with a host system, how can the GPIO be used to drive indicator LEDs to indicate charging status, fault etc? The datasheet shows how these can be programmed to inputs or outputs but how are the relevant functions assigned?

Cheers

Best answer by willzhou

Hi Jones

Yes, it can use, but different user will need different led, and special FW.

attach 1254 version is EVK board control LED example,

When TX is in charge mode LED will blink,

when rx remove, LED is on.

1 reply

willzhouBest answer
Technical Moderator
May 22, 2024

Hi Jones

Yes, it can use, but different user will need different led, and special FW.

attach 1254 version is EVK board control LED example,

When TX is in charge mode LED will blink,

when rx remove, LED is on.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.