Skip to main content
Associate II
April 23, 2024
Question

STWLC98 and STWLC38 TX Mode

  • April 23, 2024
  • 2 replies
  • 1787 views

Hello,

Is there already a solution available to use the STWLC98 or the STWLC38 in TX mode? Is there any application note or some other more detailed description for the TX mode?

 

My problem is the following:

I want to transmit 15W, but the STWBC86 can only transmit 5W. So I have to deal with the STWBC2-HP, but this one is too big for my application and has too much functionality I do not need. Furthermore it would be nice if I can use the same IC on RX and TX side.

 

Thank you

Simon

 
This topic has been closed for replies.

2 replies

Technical Moderator
April 23, 2024

Hi

STWLC98 support TX mode, please check this link at page 44 5.15 Transmitter (Tx) mode

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Technical Moderator
April 23, 2024

@simonh Do you have STWLC98 EVB board on hand?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Technical Moderator
April 23, 2024
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
simonhAuthor
Associate II
April 23, 2024

I have seen it, but it is not yet in stock at any supplier. But I think it is not possible to Transmit Power with the Evalboard without adapting it. In the Application note there is mentioned, that the parts for TX mode are not assembled.