Switch between VBAT and VDD without removing VDD
My device has various connected sensors and peripherals. The device is intended to go to sleep for extended periods of time before waking up and taking measurements. Currently, the main VDD is a large external battery and VBAT is a coin cell used to maintain the clock if VDD is depleted/removed. I'm wondering if it is possible/advisable to have the MCU control a switch to turn off VDD and thereby greatly minimize standby currents of DC/DC converters, switches, etc. and only power the MCU with the coin cell using VBAT?