Thermal and SOA protection of L78M05AB regulator ?
I have some questions regarding the L78M05AB regulator IC.

1. Could you please investigate the temperature at which this IC's the thermal protection actually activates?
2. I have been informed that the thermal protection mechanism shuts down the output voltage.
However, when we applied heat, we observed behavior suggesting that the output appears to remain at a constant level.
If the temperature is kept at a specific value, will the output remain constant (for example, 3V)?"
3. Could you please clarify the behavior when SOA protection is triggered?
Does the circuit limit the output, or does it enter a shutdown state?
4. Related to SOA protection, is there any case where the voltage is reduced and latched at a certain level?
5. Are there any restrictions or specifications regarding harmonics or noise on the input voltage of the regulator IC?