Transistor configuration for a heating mat (big load)
Hello everybody,
I am currently designing a configuration utilizing two drivers to heat a mat, which is a resistor load requiring 24V and 3.3A. This component is commuted at 100 Hz.
For this setup, I've employed two different drivers: the first one being VNB14NV04TR-E, utilized for switching large loads requiring high currents. On the other hand, I've utilized the MIC5018 to control the spoken driver. Additionally, I have add a pull-down resistor to force the 0 state, and I may use a series resistor for the PWM signal to limit the current, although I am not sure about it....
We have conducted tests of this configuration on one STM developmentboard, and it appears to be functioning properly. However, we would like to confirm if the setup is correct, as we have connected this system to a developed PCB with STM32h563, resulting in sparks and the MCU failure. The diode is a recent addition to the design; initially, we believed it might not be necessary due to the resistor load, assuming there would be no induction issues.
Apart from the current configuration, are there several circuit solutions and recommendations to prevent reverse currents or voltage spikes?
Thank you.