Triac Ripple Voltage T1250H-6I (with schematic)
Hello
I am currently developing an AC switch for a heating boiler in a coffee machine.
The boiler has a power rating of approx. 1200W.
To control the boiler, I have opted for a triac circuit (T1250H-6I) with an optotriac (14230634300) and ZCC. I used Application Note AN5114 to size the resistors. The description is generally excellent. However, I have a question regarding the voltage ripple on the triac. The note recommends a value of 4V. I cannot achieve this value with the standard resistor values available. My calculations give a voltage ripple of approx. 25V. Is that too much? Or what can I do to get down to the recommended value of 4V, triac with lower Igt?
Best regards
John