Skip to main content
NPAL.1
Visitor II
May 4, 2023
Question

TS33 datasheet mentions that it supports 1.8V fixed output voltage too, but cannot find relevant ordering code.

  • May 4, 2023
  • 1 reply
  • 597 views

..

This topic has been closed for replies.

1 reply

Peter BENSCH
Technical Moderator
May 4, 2023

Welcome, @NPAL.1​, to the community!

Unfortunately, the first overview page of the data sheet indicates voltages that are not currently supported. However, the information is relevant in the data sheet, section 7 (Ordering Information):

  • 1.25V
  • 2.048V
  • 2.5V
  • 3.0V
  • 3.3V

That means, 1.8V, 4.096V and 5V are not (yet) available.

And if you want to ask now when this will be the case - that is currently unpredictable.

Does it answer your question?

Regards

/Peter