Unable to use the EVAL6235Q alone or with the STEVAL-PCC009V2
Description:
This is what we did with the EVAL6235Q to use the external speed loop connector to drive a BLDC motor:
1. On the power supply connector, we attached 12 V.
2. We connected our BLDC motor to the 3ph BLDC motor connector.
3. We connected our BLDC motor hall effect sensors to connector J7 pins H1, H2, and H3.
4. We connected our BLDC motor power pins to connector J7 pins Vdd and GND.
5. We connected J6 pin 2 and 3 together.
6. We connected a 3.3 V, PWM (and varied the frequency between 1 to 100 kHz) from a function generator to J8 pin 3 (slout).
After doing the steps 1 to 6 above, the motor would not turn and if we watched the voltage on connector J5 pins OUT 1, OUT 2, OUT3, the voltage was always zero.
Are we doing something wrong or is there a problem with our EVAL6235Q?
This is what we did to try and get the STEVAL-PCC009V2 to work:
We purchased an STEVAL-PCC009V2 (IBU universal interface based on the STM32x) board because it was recommended to be used with the EVAL6235Q board. However, the drivers for this board are written to be used with Window XP or 2000. Our PCs are running Windows 10. In the documentation, it says that when the STEVAL board is connected to the PC that a Window will pop up to walk through installing the drivers. However, this does not happen. Also, after it is connected to the USB port and we open Device Manager and expand the “Universal Serial Bus controllers�?, the “STM32 based IBU UI Tool�? is not shown. The user manual says to contact technical support if this happens.
How should we proceed? Do you have Window 10 drivers? Or do you have an newer communication board?