Use of powerSTEP01 in “voltage mode�?
We are developing an OEM board which is capable of driving bipolar stepper motors from 15 to 80Vdc 10A max, in voltage mode and current control. Our customers should be able to change the supply voltage (Vbus), operating mode (voltage or current), without changing the assembly of the pcb.
We use powerSTEP01, and we studied AN4144 “Voltage mode control operation and parameter optimization�?, but still have a couple of questions:
- How can we use voltage compensation (see AN4144, section 1.3) in our application without having to change the resistance values of the divider bridge?
- Does the current measurement resistors (Rsens) have an influence in voltage mode? Can we leave them for both operating mode?
- Is there another way to define "Ke"? I use the method described in section 2.1 of AN4144, it works well but for OEM customers of our system it might be difficult to implement. Any suggestion?
- Is it possible to preset a maximum speed according to VS, I, L, R or Ke? If so, by what formula?
- Is there any documentation similar to AN4144 for current control?
NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.