VIPER06 no-isolated can't start (over current protection ?)
Hello,
I have designed the same schematics of the website :

The output should be 18V and no significative current (1-5mA output because MCU off).
I have tested the input voltage at [80 ; 200] V and I have the same problem. The chip try to start during 400ns and stop during 1sec.
I can confirm there is no problem on the output because I have checked the output.
The transformer is a wurth : 7508111324
The transformer parameter is :

The VCOM is always 3.3V during the start-up and it doesn't "move".
The yellow is ILIM pin and blue is DRAIN :

do you have any idea ?