Viper16LD problem
Hello,
We are facing a problem with the use of Viper16LD.
My schemtic is like following:
We already produce over 100 board without problem.
Now, on a new batch, we have a problem.
The input vlotage named "DCBus" start at 220*1.41 = 325V.
With that, Viper output is correct (about 16V)
After that, we start a PFC which increase DCBus up to 400V.
But when DCBus over pass about 360V, the Viper output 16V fall!
PLease find a Scope screen:
Could you have a check or Ideai why problem occurs?
Regards