VN5050AJ CS_DIS not working
We have a new design were we have multiple VN5050AJ high side drivers. We have connected all current sense pins together and want to enable just one current sense per time to save analog inputs. Now it seems that the CS_DIS pin is ignored and the chip always drives the correct current out of the Current_Sense pin and ignoring the CS_DIS. Levels should be fine as we have 0 Volts and 3.3V for the CS_DIS input (Pin 5) which is way above the limits from the Datasheet. 0.9 and 2.1V.
Thanks