Why does the LD39050 have a maximum capacitance value?
We have been seeing some intermittent failures of the LD39050 in our products.
I can't see anything wrong with the design other than the output capacitance.
The datasheet specifies a maximum of 22uF for stability, but our design has approx 30uF on the board.
I have tested the stability of the LD39050 by step changing the load, as well as introducing step changes on the inputs. I've done this testing with reduced output capacitance (~10uF), as well as increased output capacitance (~50uF) and I see no stability issues. If anything, the greater capacitance was more stable.
When the part fails it loses regulation. We are running the adjustable version stepping 5V down to 3.3V. When it fails, the LD39050 feels hot and the output is 4.5V.
I am completely out of ideas so I am hoping someone will have some to share!