Skip to main content
ARodr.12
Associate
May 3, 2022
Solved

Why STEVAL-SPIN3201 not work without USB

  • May 3, 2022
  • 2 replies
  • 1319 views

Hi,

I have kit STEVAL-SPIN3201 and now i have a expirience with controling my motor. But i never was able to start board without USB cable. It's seems like board need USB voltage for start microcontroller. So it can not start without USB. But if i then remove the USB, it works. But if i push the RESET button later, it does not work again until restarting kit with USB. So i need understand why it becouse in future i want to design my pcb.

This topic has been closed for replies.
Best answer by Cristiana SCARAMEL

Hello @ARodr.12​ and welcome to the ST Community.

The STSPIN32F0 RESET signal (NRST) is connected to the ST-LINK reset (T_NRST) through the jumper J8.

Try to open J8 jumper and check if STSPIN32F0 operation is independent by USB connection.

Let me know your feedback.

2 replies

Cristiana SCARAMEL
Technical Moderator
May 4, 2022

Hello @ARodr.12​ and welcome to the ST Community.

The STSPIN32F0 RESET signal (NRST) is connected to the ST-LINK reset (T_NRST) through the jumper J8.

Try to open J8 jumper and check if STSPIN32F0 operation is independent by USB connection.

Let me know your feedback.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Visitor II
November 17, 2023

Hello

Same problem,  STEVAL-SPIN3201 does not start without usb power.  If J8 is open, need to press reset button after connecting usb, if  J8 is short- no need to press reset, its reset automatically. After board is starting, no need usb power anymore.

Example is standart from MotorControl Workbench 6.1.2

 

ARodr.12
ARodr.12Author
Associate
May 10, 2022

Thank you! It work. Moreover, i found a bug in my program.

Cristiana SCARAMEL
Technical Moderator
May 11, 2022

Hi @ARodr.12​, good!

I’m glad everything is working.

Remember to "Select as Best" label in the proper reply to your original question.

So, you can help others Community member to find the answer at similar question.

"If you feel a post has answered your question, please click ""Accept as Solution"""