WLC38 - compatible chargers
Hi,
We are developing a product using the WLC38 as RX.
It works OK in combination with wbc2tx50 board, and a single Spigen QI charger we found (no overheating, constant power > 10W achievable).
However using any other charging pads (either Qi1 15W or Qi2..) either doesn't communicate to the EPP mode (stays in BPP) or is working for ~10 seconds, but after that shuts down (seems like they try to communicate higher OP frequency, which causes wlc38 to overheat, or trigger some other protection...)
Question:
Can anybody recommend any changes in configuration of WLC38 to support more charging pads? Allow EPP mode, and allow continous operation?
Are there any known and available chargers that are tested, and work ok with WLC38 in EPP up to 15W?
Looking through the forum
Thanks in advance!